cancel
Showing results for 
Search instead for 
Did you mean: 

BUG in AZRTOS 6.4 NetxDuo v3.3

mbarg.1
Associate III

in file app_netxduo.c

function static VOID nx_app_thread_entry (ULONG thread_input){ ....

/* wait until an IP address is ready */ if(tx_semaphore_get(&DHCPSemaphore, TX_WAIT_FOREVER) != TX_SUCCESS)

blocks code execution

as in function tx_semaphore_create(&DHCPSemaphore, "DHCP Semaphore", 0){

"tx_semaphore_put(&DHCPSemaphore);"

has been removed - was present in previous versions - nothing sets this semaphore

0 REPLIES 0