2025-01-23 3:11 PM
Hi,
I was able to run a demo project on a STM32H573 dev board. I am using ThreadX and NetxDuo, with mqtt addon.
I was able to connect to the mqtt broker and send/receive messages.
I want also to be able to use the bsd sockets to send packets on layer 2. As far as I have understood, for sending and receiving layer 2 packets I need to use bsd sockets.
I followed the doc from github, added the files .h and .c
I had to add the line
#define TX_THREAD_USER_EXTENSION int bsd_errno
in the user code part of "tx_user.h", so it can survive a code generation.
Then I enabled
NX_ENABLE_EXTENDED_NOTIFY_SUPPORT
and
NX_ENABLE_IP_RAW_PACKET_FILTER
Then I got into a problem: the redefinitions of structs and function names, so I added
#define NX_BSD_ENABLE_NATIVE_APIin the user code part of "nx_user.h"
I want to have raw support, so I also added
#define NX_BSD_RAW_SUPPORTin the user code part of "nx_user.h"
Now I get an error when I compile:
"nxd_bsd.c:474: undefined reference to `_nx_driver_hardware_packet_received_callback' "
Am I missing something or I am doing it wrong?
Thanks in advance tor any help
2025-01-24 3:02 PM
Ok, I got something in working condition.. kinda. I can init and create a raw socket.
Now, if I call the function "nx_bsd_send", the compiler is complaining abount this:
../NetXDuo/App/nxd_bsd.c:13327: undefined reference to `_nx_driver_hardware_packet_send'that line is in the function
static INT _nx_bsd_hardware_internal_sendto(NX_BSD_SOCKET *bsd_socket_ptr, CHAR *msg, INT msgLength, INT flags, struct nx_bsd_sockaddr* destAddr, INT destAddrLen)If I go to that line and press F3, I go to the declaration in nxd_bsd.h file:
extern UINT _nx_driver_hardware_packet_send(NX_PACKET *packet_ptr);If I press again F3, I go straight to the implementation in the file "nx_stm32_eth_driver.c".
How is it possible for the ide to find the function, but when I compile I get undefined reference?
Thanks for any hint or advise
2025-02-17 8:19 AM
Hello @coso2 ,
This is clearly an include path problem it's normal that IDE recognizes the function and the compiler doesn't as it needs to have a path to the file where the function was declared.
Regards
2025-02-18 1:53 PM - edited 2025-02-18 1:54 PM
The function "_nx_driver_hardware_packet_send" in "nx_stm32_eth_driver.c" is static
static VOID _nx_driver_packet_send(NX_IP_DRIVER *driver_req_ptr)
And every time I generate the code, I have to manually remove the "static" keyword
2025-02-24 10:27 AM
I am having the exact same issue.
The function "_nx_driver_hardware_packet_send" in "nx_stm32_eth_driver.c" is static and the "nxd_bsd.h" file has that function externed. Therefore, the only way for this addon to work is to go and edit the file every time.
NXD_BSD also externs `_nx_driver_hardware_packet_received_callback` when we enable NX_BSD_RAW_SUPPORT. This function doesn't seem to exist at all in the ethernet driver.
Does ST have any instructions for integrating the NXD_BSD addon into a H7 project using the NX_BSD_RAW_SUPPORT defined? This flag seems to be required if you want to support multicasting.