2023-12-21 6:13 AM
I am looking forward to making a flight controller using STM32H7ZGT6. But I am in confusion that can I use FTDI FT232RL to program the H7 board which is a USB to Serial Converter. Please help me out, Can I use FT232RL.
Thanks.
Solved! Go to Solution.
2023-12-21 8:05 AM
I don't know, can you? It is technically possible, but do you have the skills necessary to do that? Probably not a great choice when a $10 solution exists. Not that obtaining the st-link firmware may be problematic as it isn't published by ST.
2023-12-21 6:28 AM
Hello @23Prathmesh
Here is an example project shared by one of our customers using FT232RL
Can I drive a 1280×720 display with the STM32H7x7? - STMicroelectronics Community
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-21 6:28 AM
Use a programmer such as ST-LINK/V3MINIE with a SWD connection to the board for development.
You can program a chip over UART using the built-in bootloader, but you cannot debug it and therefore you cannot develop efficiently.
2023-12-21 7:58 AM
Can I create my own ST-LINK PCB Board programmer ?
2023-12-21 8:05 AM
I don't know, can you? It is technically possible, but do you have the skills necessary to do that? Probably not a great choice when a $10 solution exists. Not that obtaining the st-link firmware may be problematic as it isn't published by ST.
2023-12-21 8:21 AM
Thanks