cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding ST-Link access on evaluation board STM32F769I-EVAL

rdevisetti
Associate III

Please let me know if normal USB cable can be used to connect to STM32F769I-EVAL board, load and debug the code or do we need to connect any other cable only for debugging purpose. Please reply with details.

Thanks,

 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

All you need is a Micro USB/USB Type A cable. 

USB cable.jpg

Please be sure it's a data cable not just to power devices.

Connect it to this USB connector on the board:

SofLit_0-1703235570553.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @rdevisetti 

You have to use a data cable not just for example a phone USB cable or other type of cables to make sure everything works fine.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

mƎALLEm
ST Employee

Hello,

All you need is a Micro USB/USB Type A cable. 

USB cable.jpg

Please be sure it's a data cable not just to power devices.

Connect it to this USB connector on the board:

SofLit_0-1703235570553.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.