2024-10-25 12:54 AM - edited 2024-10-25 07:16 AM
I have develop a program on STM32F746G-DISCO revision B02 with QSPI N25Q128A13EF840E
Now the new boards revision C03 use the QSPI W25Q128JVEIQ.
I have copied the file W25Q128JVEIQ_STM32F746G-DISCO.stldr from CubeIDE 1.16 to the STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader but the external loader is not flash.
I need to change some in my code to use this new QSPI chip ?
Solved! Go to Solution.
2024-10-25 05:49 AM
The BSP initialization, STM32 side, will need slightly different code to work into 4 pin, 4 bit operations. The commands and status registers between the Micron and Winbond are subtly different.
Code for the images to work needs to get the memory IC into memory mapped mode, and you perhaps need to verify you can read the content and that that matches expectations.
I'd perhaps use a CRC as a quick check of integrity. ie data built on host matchs data visible on the target.
2024-10-25 05:55 AM - edited 2024-10-25 05:57 AM
@Ciuffoly www.audiodesignguide wrote:
STM32F746G-DISO ver. B-04 with N25Q128A13EF840E
14:09:22 : Data read successfully
14:09:22 : Time elapsed during the read operation is: 00:00:00.007
14:09:25 : Memory Programming ...
14:09:25 : Opening and parsing file: FinalMono_ver5.hex
14:09:25 : File : FinalMono_ver5.hex
14:09:25 : Size : 1.52 MB
14:09:25 : Address : 0x08000000
14:09:25 : Erasing memory corresponding to segment 0:
14:09:25 : Erasing internal memory sectors [0 2]
14:09:26 : Erasing memory corresponding to segment 1:
14:09:26 : Erasing external memory sectors [0 23]
14:09:29 : Download in Progress:
14:09:40 : File download complete
14:09:40 : Time elapsed during download operation: 00:00:15.030STM32F746G-DISO ver. C-03 with W25Q128JVEIQ
14:16:59 : Data read successfully14:16:59 : Time elapsed during the read operation is: 00:00:00.01314:17:00 : Memory Programming ...14:17:00 : Opening and parsing file: FinalMono_ver5.hex14:17:00 : File : FinalMono_ver5 (6).hex14:17:00 : Size : 1.52 MB14:17:00 : Address : 0x0800000014:17:00 : Erasing memory corresponding to segment 0:14:17:00 : Erasing internal memory sectors [0 2]14:17:01 : Erasing memory corresponding to segment 1:14:17:01 : Erasing external memory sectors [0 23]14:17:07 : Download in Progress:14:17:27 : File download complete14:17:27 : Time elapsed during download operation: 00:00:27.461but still no images loaded from QSPI
To me this is no more an issue with the external bootloader. It's something related to QSPI inti in your application.
I invite you to close this thread and open an new one for the second question.
2024-10-25 06:31 AM - edited 2024-10-25 07:17 AM
I have found an information about this problem so the action to solve is here:
1) download the last driver in the en.stm32cubef7-v1-17-2.zip archive with inside the w25q128j.h file
2) put this w25q128j directory inside \Drivers\BSP\Components
3) save previous stm32746g_discovery_qspi.c and stm32746g_discovery_qspi.h
4) copy new files stm32746g_discovery_qspi.c and stm32746g_discovery_qspi.h from ...v1-17-2.zip archive
5) add in the MCU GGC Compiler Preprocessor define the USE_STM32746G_DISCO_REVC03
6) recompile
Now also ST-LINK work !
2024-10-25 07:12 AM
you can also use the cube programmer to read the external flash to see if the image is really loaded into the external flash