cancel
Showing results for 
Search instead for 
Did you mean: 

[SOLVED] I cannot flash and use the QSPI W25Q128J chip on the new STM32F746G-DISCO version C03

I have develop a program on STM32F746G-DISCO revision B02 with QSPI  N25Q128A13EF840E

Now the new boards revision C03 use the QSPI W25Q128JVEIQ.

I have copied the file W25Q128JVEIQ_STM32F746G-DISCO.stldr from CubeIDE 1.16 to the STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader but the external loader is not flash.

I need to change some in my code to use this new QSPI chip ?

 

Ciuffolywwwaudiodesignguide_0-1729843256117.png

 

13 REPLIES 13

The BSP initialization, STM32 side, will need slightly different code to work into 4 pin, 4 bit operations. The commands and status registers between the Micron and Winbond are subtly different.

Code for the images to work needs to get the memory IC into memory mapped mode, and you perhaps need to verify you can read the content and that that matches expectations. 

I'd perhaps use a CRC as a quick check of integrity. ie data built on host matchs data visible on the target.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Ciuffoly www.audiodesignguide wrote:

STM32F746G-DISO ver. B-04  with N25Q128A13EF840E

14:09:22 : Data read successfully
14:09:22 : Time elapsed during the read operation is: 00:00:00.007
14:09:25 : Memory Programming ...
14:09:25 : Opening and parsing file: FinalMono_ver5.hex
14:09:25 : File : FinalMono_ver5.hex
14:09:25 : Size : 1.52 MB
14:09:25 : Address : 0x08000000
14:09:25 : Erasing memory corresponding to segment 0:
14:09:25 : Erasing internal memory sectors [0 2]
14:09:26 : Erasing memory corresponding to segment 1:
14:09:26 : Erasing external memory sectors [0 23]
14:09:29 : Download in Progress:
14:09:40 : File download complete
14:09:40 : Time elapsed during download operation: 00:00:15.030

STM32F746G-DISO ver. C-03  with W25Q128JVEIQ

 

  14:16:59 : Data read successfully
  14:16:59 : Time elapsed during the read operation is: 00:00:00.013
  14:17:00 : Memory Programming ...
  14:17:00 : Opening and parsing file: FinalMono_ver5.hex
  14:17:00 :   File          : FinalMono_ver5 (6).hex
  14:17:00 :   Size          : 1.52 MB 
  14:17:00 :   Address       : 0x08000000 
  14:17:00 : Erasing memory corresponding to segment 0:
  14:17:00 : Erasing internal memory sectors [0 2]
  14:17:01 : Erasing memory corresponding to segment 1:
  14:17:01 : Erasing external memory sectors [0 23]
  14:17:07 : Download in Progress:
  14:17:27 : File download complete
  14:17:27 : Time elapsed during download operation: 00:00:27.461

but still no images loaded from QSPI

 

 


To me this is no more an issue with the external bootloader. It's something related to QSPI inti in your application.

I invite you to close this thread and open an new one for the second question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

I have found an information about this problem so the action to solve is here:

1) download the last driver in the en.stm32cubef7-v1-17-2.zip archive with inside the w25q128j.h file

2) put this w25q128j directory inside \Drivers\BSP\Components

3) save previous stm32746g_discovery_qspi.c and stm32746g_discovery_qspi.h

4) copy new files stm32746g_discovery_qspi.c and stm32746g_discovery_qspi.h from ...v1-17-2.zip archive

5) add in the MCU GGC Compiler Preprocessor define the    USE_STM32746G_DISCO_REVC03

6) recompile

Now also ST-LINK work !

 

you can also use the cube programmer to read the external flash to see if the image is really loaded into the external flash