2025-01-27 4:10 AM - last edited on 2025-01-27 5:46 AM by Andrew Neil
For more than 3 days I am trying to solve a problem of connecting to Riverdi board using external ST-link from a discovery board. I flashed apps without problem and now I can't do anything. I remember last time I was flashing an app it asked that firmware of St-link has to be updated before continuing so I proceeded. I successfully flashed the app but now I am unable to flash it again.
13:07:23 : STM32CubeProgrammer API v2.18.0 | Windows-64Bits
13:07:27 : UR connection mode is defined with the HWrst reset mode
13:07:27 : ST-LINK SN : 0670FF3332584B3043153854
13:07:27 : ST-LINK FW : V2J45M31
13:07:27 : Board : STM32F4DISCOVERY
13:07:27 : Voltage : 2.91V
13:07:27 : Error: Unable to get core ID
13:07:27 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
If I try to connect to other boards It is connected without problem.
Please help,
Regards
2025-01-27 5:11 AM - edited 2025-01-27 5:18 AM
Hello,
Which board? in the title you said: "STM32H7 cant connect to board"
but the log said: Board : STM32F4DISCOVERY
Could you please clarify? do you have a F4 discovery board connected via USB to your PC?
2025-01-27 5:42 AM
That is the weird thing , this is the ST-link from F4 discovery board, I removed the jumpers to use only ST-link. I performed connect under Reset and performed full chip erase. However, flashing is still not possible.
2025-01-27 5:48 AM - edited 2025-01-27 5:57 AM
@richi wrote:
That is the weird thing , this is the ST-link from F4 discovery board,
Not clear. Are you using a STLINK module from F4 discovery to connect to that Riverdi board? If yes that was an important information you should provided in the first post.
2025-01-27 5:48 AM
2025-01-27 6:09 AM
Riverdi board only offers block diagram:
On the stm32f4 side I just removed jumpers and connected pins 2,3,4,5,6 , VCC is given from an external power supply on through a power connector.
I was reading on internet that MCU could be bricked if I accidentally re-configured SWD pins for some other alternate function, what is the procedure if that is the case?
2025-01-27 6:25 AM
None of that shows us the actual connections that you have made between your disco & riverdi boards.
@richi wrote:I was reading on internet that MCU could be bricked if I accidentally re-configured SWD pins for some other alternate function
Not really "bricked" - but inaccessible to SWD.
@richi wrote:what is the procedure if that is the case?
2025-01-27 12:13 PM
Can you please tell me how can I flash a program from STMCubeProgrammer but with 2 hex files. One is for internal flash starting at 0x08000000 and one for external flash 0x090000000, earlier I would just click on flash in TouchGFX and everything would be done automatically.
2025-01-28 12:27 AM
That's a separate question - you need to be able to connect to the board first!
Have you now got the connection working?