Skip to main content
Associate
January 21, 2025
Solved

STM32H725 SMPS issue

  • January 21, 2025
  • 3 replies
  • 3441 views

I am having and issue with a STM32H725RGV6.

After powering my board, I can see the SMPS output at 1.36V, which I have connected to the VCAP inputs.
I can also connect to the µC using the STM32CubeProgrammer.

However, after flashing a simple firmware, the SMSP output drops to 0V and I can not connect anymore. I am aware that this can be the result of an improper SMPS configuration (https://community.st.com/t5/stm32-mcus/unable-to-connect-to-stm32h7-devices/ta-p/49296). However, in my (cube generated) project am am calling

HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY)

so this should be correct. Additionally, I tried to upload a program with nothing but an infinite loop in main, and the problem still occurs.

When pulling BOOT0 high, the SMSP output becomes 1.36V again and I can connect again. This makes me believe, that everything is set-up correctly hardware-wise. Otherwise, the bootloader would not run.

thank you for your help

STM32H725RGV6 power.png

 

This topic has been closed for replies.
Best answer by mƎALLEm

Hello @BenUtzer and welcome to the community,

If you are using CubeMx to generate the code, I think you have the same issue as these threads:

Thread1

Thread2

Please confirm.

3 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
January 21, 2025

Hello @BenUtzer and welcome to the community,

If you are using CubeMx to generate the code, I think you have the same issue as these threads:

Thread1

Thread2

Please confirm.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
BenUtzerAuthor
Associate
January 21, 2025

Thank you very much. I can confirm that this was indeed the issue.

mƎALLEm
ST Technical Moderator
March 6, 2025

Issue fixed in CubeMx 6.14.0 (already available on ST website)

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.