cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting issue Nucleo-H7A3ZI - Q

Durgasish
Associate II

Hello I can't able to connect my NUCLEO - H7A3ZI -Q. Its showing error while commenting.

Durgasish_0-1724824641884.png

Please help me with solving this issue.

20 REPLIES 20

Hello @STTwo-32  Still not able to solve the issue I'm facing the same thing

 

If you use STM32CubeProgrammer, what message you get?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@Durgasish wrote:
AndrewNeil_1-1724837505880.png

So did you do that?

Also:

AndrewNeil_2-1724837554027.png

Does that apply to you situation? If so, did you do it?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Yes I did that way.

 

@mÆŽALLEm This what I'm getting.

Durgasish_0-1724909811339.png

 

Hello,

Is that board you face issues with, brand new?

Otherwise, you said: "No It is not modified by anyone." but did someone use it apart of you? so you can't be sure if it was modified or not.

Could you please share two clear photos of your board top and bottom?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Image.jpg

Image (1).jpg

 Here are the pictures of top and bottom of my board.

Hello,

just in case, please have a look to that article:

Unable to connect to STM32H7 devices  

I tired with solution 1 its not working
And as per solution 2:
how can I ensure that the BOOT_CM7_ADD1 configuration is set to point to the system memory.? Can you please help me with it.

Visually, I don't see issue on the board according to the images you shared.

For Solution 1, please check again by following this article:

https://community.st.com/t5/stm32-mcus/how-to-unbrick-an-stm32h7-after-setting-the-wrong-power-mode/ta-p/49691

BOOT_CM7_ADD1 is not accessible as it's located in option bytes and you couldn't connect to the board with STM32CubeProgrammer to check.

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.