ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R3914 Read/Write to Tag

All, I would like to first begin with saying thank you for your time in attempting to assist me.Library used: NFC st25r3911b LibraryI am attempting to read and write from/to a tag; more specifically a Type-2 and Type-4. I have been looking through ex...

APant.2 by Associate III
  • 5019 Views
  • 12 replies
  • 0 kudos

Resolved! ST25R3916B Failing to Respond on SPI

Hi,I am using the ST25R3916B on a custom PCB and am having some field failures where it seem that the device is failing to respond on SPI to my microcontroller.  When I get the board back in house I can see that my first SPI command to read the ID re...

Resolved! st25r3918

Hi, I have been working on a project where i use st25r3918. However, I could not make it work. I have checked my hardware by using other boards and it looks like it is working. For sorftware, I have tried using st25r3911's library and have changes ac...

MimiTrn by Associate
  • 670 Views
  • 1 replies
  • 0 kudos

Resolved! Help finalizing custom Rust driver (st25r3911b)

Hi! A while back I started writing Rust driver for st25r3911b chip. Currently, it works and can read 14443A chip. The issue is that compared to official software (Discovery GUI) the read distance is about half. So if official software reads at 8-9cm ...

RMuiz.1 by Associate III
  • 3077 Views
  • 11 replies
  • 0 kudos

Resolved! ST25RU3993-HPEV kit

I bought ST25RU3993-HPEV kit to make my project. I try to program the programming board STM32L476RGT6 MCU in CUBE IDE (Not showing board). Then I try STSW-ST25RU001 (ST25RU3993 Reader suite), But not working as well, not reading and writing tags. My ...

RBhav.1 by Associate
  • 845 Views
  • 1 replies
  • 0 kudos

Resolved! ST25R3911B with FreeRTOS

Hi everybody, I need to integrate the ST25R3911B NFC reader (X-NUCLEO-NFC05A1 a.t.m.) into a project with STM32H735G running FreeRTOS (with a TouchGFX task and another peripheral task running ). https://community.st.com/t5/st25-nfc-rfid-tags-and-read...

SScar.2 by Senior
  • 2408 Views
  • 3 replies
  • 1 kudos