ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CR95HF with STM8L

Posted on March 24, 2016 at 08:46In AN3985 application note , it mentions that using CR95HF with STM8L-Discovery board. May I know where to download this firmware ? which show STM8L mcu work with CR95HF read/write tag. Thx #cr95hf

So.Sunny by Associate II
  • 547 Views
  • 1 replies
  • 0 kudos

Resolved! M24SR ExtendedReadBinary command

Posted on March 03, 2016 at 03:33Hi, I want to use the ExtendedReadBinary command, but go through all demo App and can't find it . Can you advise it belong to which class in the M24SR demo App ?Thanks  #m24sr-issue

So.Sunny by Associate II
  • 502 Views
  • 1 replies
  • 0 kudos

Resolved! ST25 Android app SendInterrupt bug

Posted on February 27, 2016 at 02:42 Hi, I have downloaded the source code for the ST25 demo Android app (1.0.2), and have found a bug with the SendInterrupt command inType4Tagm24sr7816STCommands.java: // SendInterrupt command ...

Resolved! M24SR04 EEPROM direct access

Posted on February 24, 2016 at 08:57Hi all, I'm using a M24SR memory connected by I2C bus to a Freescale M0 microcontroller. Given that the free space for the firmware is very little, I have problems integrating the ST library for reading and writin...

Resolved! Number of NDEF files on ST25TA64K

Posted on December 08, 2015 at 01:22The default configuration has 1 NDEF file that occupies the entire memory. Is it possible to slice up the memory between 2 or more NDEF files?  If more than one file can be created, what is the maximum number of f...

calai by Associate
  • 885 Views
  • 3 replies
  • 0 kudos

Resolved! Verification of antenna/distance

Posted on February 02, 2016 at 13:48Hello.How do I know that my design is good enough for all kinds of phones? We have the PCB inside a cabinet, where the phones can max be as close as 3-4cm to the antenna, (a PCB-antenna and a M24LR). How do we ver...

na by Associate II
  • 577 Views
  • 1 replies
  • 0 kudos

Resolved! Communication with M24SR over I2C

Posted on January 22, 2016 at 10:18Hi everyone, i try to connect M24SR chip with my MarS Board i.MX6 I didn't try to configure my inputs and outputs, just try to use it with command, that already exists in Linux.  For example with ''write()'' and ''...

Resolved! I2C Watchdog

Posted on January 26, 2016 at 17:17Hello, I'm interested in the ''I2C Watchdog'' setting in the M24SR System file. There doesn't seem to be any information in the datasheet about it, and I couldn't find anything using google either. Anyone know if a...