2016-02-23 11:57 PM
Hi all,
I'm using a M24SR memory connected by I2C bus to a Freescale M0 microcontroller. Given that the free space for the firmware is very little, I have problems integrating the ST library for reading and writing access to the NDEF files. So, I was wondering if it was possible to access the EEPROM memory directly without using the ISO-DEP protocol, but accessing to the locations of the EEPROM memory with standard I2C command. In my firmware I only have to access to a NDEF text file for reading and read the first 10 bytes of this file. So I ask you:Thank you all in advance
Daniele #read-access #m24sr #eepromSolved! Go to Solution.
2016-03-02 3:13 AM
Hello Daniele,
M24SR is accessible on the I2C side in the same manner than from the RF side. It is not possible to access the EEPROM as a standard EEPROM memory.Best regards,Have a good day2016-03-02 3:13 AM
Hello Daniele,
M24SR is accessible on the I2C side in the same manner than from the RF side. It is not possible to access the EEPROM as a standard EEPROM memory.Best regards,Have a good day