Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.
I am attempting to design a low power application utilizing the tag detection mode of the ST95HF.When operating in reader mode, performance is excellent, I am able to communicate with tags reliably at reasonable range (approx 50mm).However when attem...
We are currently developing a system for a secure door lock and we have decided to use as a key either an NFC tag or an iButton. The product must be CE certified. The NFC seems the most attractive solution, but it's certification looks to be a painfu...
Hi,We are using ST25R3911B IC in our product and I would like to know if there are any legal issues if we are implementing DESFIRE support on this chip (as it belongs to NXP)? Support guy from NXP told us if we want to support DESFIRE we should use a...
Hey there , I have just revived ST25R3911B disco board. For the testing purpose I'm using ST25-pc and GUI app. I can get the UID for the ISO14443A and ISO15693 , but my ultimate goal is to read and write the selected sector of Mifare 1K...
I am using a Raspberry Pi with the rfal_1.3.0 libraries and with the demo software I can get the board to read iCode Tag UIDs without any problem.However, I want to be able to read and write from the iCode tags memory, but I can’t find the commands w...
Hi, I'm really new in this world but I'm trying to read a NFC card with my NFC01A1 on a Nucleo L476RG but all the examples I found are only for writing on an android phone. Is it possible to read a NFC card with the NFC01A1 ? And if yes, how ? Is the...
I generated a new cube project, included everything what nfc reader needed(like the sample project for 401), I modified the platform.h, the SPI is working, but its a bit confusing, because if I use HSI the reading is freezing in demoPollNFCA() - wit...
Unable to get ST25RU3993-EVAL Board as it does not appear to be available, have all the details of board if we construct this Evaluation board would we be able to load the firmware into it and use the PC software and it work ok?Second question, there...
Hello,I am working on a project based on NFC energy harvesting application. I am using AMS AS3955 dynamic tag which offers this functionality with ST25R3911B as the reader. In the ST25R3911B datasheet, it says that NFC type 4 tags are preferred and ...