ST25 NFC/RFID tags and readers

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Solved: Another mistake in M24SR datasheet

Posted on April 02, 2014 at 12:27Hi, as [DEAD LINK /public/STe2ecommunities/memories/Lists/M24SR%20Series/Flat.aspx?RootFolder=/public/STe2ecommunities/memories/Lists/M24SR%20Series/M24SR%20-%20mistake%20in%20table%2067%20Datasheet&FolderCTID=0x0120...

joaquim by Associate III
  • 767 Views
  • 3 replies
  • 0 kudos

Resolved! Demo CR95HF-A ISO 15963 max range

Posted on January 23, 2014 at 11:23Hi, I'm trying to achieve the maximum reading range from my demoboard CR95HF-A with a ISO 15693 tag (LRi2K). Until now I've obtained best results with modulation-index 10% and gain 34dB by writing 0x50 to ARC_B reg...

pieretti by Associate II
  • 1897 Views
  • 13 replies
  • 0 kudos

Resolved! M24LR04E-R time to ready from power-up?

Posted on March 17, 2014 at 12:24Hi all, I'm looking for an indication of worst-case time-to-ready: i.e. from power-up - assume external VCC, not induced power - to fully commandable from I2C. I've searched the datasheet (DocID022208 rev 8) from end...

Resolved! Bug in CR95HF development software

Posted on March 19, 2014 at 13:44First of all: I really like the software for DEMO-CR95HF-A. But there is an issue with the scripting tool: The command CR95HF_ISO14443-A_SEND_APDU, 00A4040007a0000000030000 should be translated intoCR95HFDLL_SENDRECV...

Resolved! m24lr64e first time programming/ reading

Posted on March 06, 2014 at 14:50Hi, We have a custom board made using M64LR64E. Using an android phone, without powering up, will the EEPROM work directly as a NFC tag? Or should it be programmed/ configured first using I2C? We are unable to detec...

muralik by Associate
  • 462 Views
  • 1 replies
  • 0 kudos

Resolved! presence of multiple tags

Posted on March 05, 2014 at 21:04Hi. I am using CR95HF. I need to identify the presence of multiple  iso15693 tags ( placed on the same time ). I need to know how the amount of tags only. Is ther a command or algorithm ?. Please Advise. Ephraim Oved...

eoved by Associate
  • 493 Views
  • 1 replies
  • 0 kudos