Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.
Hello, I'm currently looking into the ST NFC Eval boards, as I'm planning a small project involving NFC and dataloggers. For my needs the NFC04A1 should be perfect, so I am looking at the drivers and example codes given in X-CUBE_NFC4. In the nfc04a...
I am using STM32F401RE and M24SR64-Y to read data from or write data on Mifare tags, and I have some questions, Can I use X-CUBE-NFC4 software with M24SR64-Y ? , as on your site the only compatible software is X-CUBE-NFC1.So, please can you explain t...
I used one CR95HF demonstration board USB on computer ,it's work well, but : CR95HF.dll library CR95HFDLL_USBconnect() Returned value: lngStatus: 0: is connected and ready to be used ; 1: not connected; I don't how to deal with 2 USB CR95HF on sam...
我现在使用一个DEMO-CR95HF-A usb在电脑上软件是没有问题的,但用两个USB连接时�?知�?�如何作开�?�区分,CR95HFDLL_USBconnect Returned value: lngStatus: 0: is connected and ready to be used ; 1: not connected; 如果是两�?�USB读�?�器如何区别是哪�?�USB?(if two or more USB connect ,how to deal with ?) 如何�...
Hello All,I have some CR95HF Antenna Design Queries1) what is actual difference between in performance of 424nH antenna and 1120nH antenna used in M24L-DISCOVERY kit and NUCLEO-NFC03A1 respectively?2) In CR95HF-A demo Board Antenna impedance design ...
Hi All,I'd like to use ST25DV NFC chipset on my STM32F103x project.I have found there was X-NUCLEO-NFC04A1 evaluation kit of ST25DV supporting CubeMX.I'd like to include the firmware package of NFC04A1 on my CubeMX project to use its API.How can I do...
Hello I am gonna use ST25R3916 for NFC in our products, but I am wondering that if the ST25R3916 is compatible with NXP's tag/reader? I remember that NXP's tag/reader has it's own encryption for communication... so I worry that ST25R3916 can't...
I evaluate ST25R3916 by using ST25R3916-DISCO kit and STSW-ST25R010.In Antenna features tab, I confirmed AAT_A and AAT_B values changed for tuning when a piece of metal is approached to the antenna, but in poling tab, these value did not change whe...