Upgraded ST-Link to V2.J29.M18 STM32 Debug+Mass storage.STM32 ST-LINK Utility is v4.2.0.0 USBDriver v5.0.3.0 CLI.exe v3.2.0.0Removed both ST link jumpers .Fresh CR2032 battery installed on STEVAL-SmarTag1Connected directly on SWD (pin 1 c...
Thank you for your suggestion. I am running a datalogger along with this LIS2DH12. My plan was to completely remove power from this chip to maximize the lithium coin cell life. It was my misread of the spec sheet that missed the INT1 as a push-pull ...
Thanks Luca.I followed all your suggestions without connecting.I then tried both plugging in the Smartag1 directly to the ST-Link SWD and using the 6 wire cable with the Blue wire connected to CN3-Rx as shown in the photo.I always get the NODE_L476RG...