ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Energy Harvesting/VCC issue on the NFC04A1...

Hello, I have an issue with the energy harvesting functionality on the NFC04A1, which I believe probably has a very simple solution. If the reader is kept on the tag then EH is happening and working fine, then if i take the reader away from the tag, ...

Resolved! ST25DV_Discovery_ANT_C1 High Current Draw

I have the discovery boards for the ST25DV and noticed a much higher current draw than I expected. In power down mode, (LPD = 1), the board was still drawing ~165uA.Looking at the schematics for the board, there is a 20k pullup resistor on the GPO li...

JPetr by Associate
  • 522 Views
  • 1 replies
  • 0 kudos

Resolved! cr95hf won't pole after idel command

Hi i am using an cr95hf. After using an idel command and waking up afterwards any command I send after the idle wont work. I don't even get a polling response. Unfortunately I can't find anything in the cr95hf datasheet telling me if i need to reset ...

MUnge by Associate II
  • 3859 Views
  • 23 replies
  • 0 kudos

Resolved! NFC04A1 - NFCTAG_Init function

Hello, I'm currently looking into the ST NFC Eval boards, as I'm planning a small project involving NFC and dataloggers. For my needs the NFC04A1 should be perfect, so I am looking at the drivers and example codes given in X-CUBE_NFC4. In the nfc04a...