ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R3911B- DISCO advice

Hey,I want to test an off the shelf Molex NFC antenna 15*15 mm using the ST25R3911B. Is it possible to connect the antenna to the discovery board as I wanna evaluate the antenna whilst connected to the ST25R3911B? If so, how can I test the setup? If ...

Csxhades by Associate
  • 431 Views
  • 2 replies
  • 1 kudos

Resolved! rfalFieldOnAndStartGT returns 12

I am using st25r3911b with an esp32, it works fine when i use the disco board (the original stm microcontroller desoldered). But then I decided to make my own circuit as shown in the attached image. The rfalNfcInitialize() function returns errors 0, ...

Resolved! FTM initialisation in Dynamic Tag side

I'm trying to establish communication -  FTM between ST25R3911B and ST25DV64KC . I'm running the example program in the reader module and I have enabled the mailbox in the dynamic tag side. The reader is able to detect the dynamic tag and is trying t...

hazin by Associate III
  • 442 Views
  • 1 replies
  • 0 kudos

Resolved! M24LR64E-R read with flutter

Hello, I'm having trouble reading single blocks in the M24LR64E-R tag I'm developing the app in Flutter and I'm trying to send the command in the following structure final command = [ flags, // flags 0x20, // Command: "Read Single Block" ...uid,...

Resolved! ST25PC-NFC Connecting to FEIG-CPR30

Hello, I am trying to get the ST25PC app to connect to a FEIG-CPR30-LCN9620 which I believe should be supported; however I not able to get the correct drivers to do so(Which I believe is the problem); I downloaded the most recent drivers from Feig we...

billyb_0-1733746509062.png billyb_1-1733746687215.png billyb_2-1733746708615.png
billyb by Associate
  • 623 Views
  • 2 replies
  • 1 kudos

Resolved! Mailbox Password Crash

Hello, I am trying to enable the Mailbox functionality on ST25DV64KC-DISCO board. I am using the NFCTap project,And inside it added my own storyboard and a View controller.This view controller first detects a tag at launch in view didload,then it fet...

Screenshot 2024-12-03 at 14.24.54.png
Aly by Associate III
  • 408 Views
  • 1 replies
  • 0 kudos