ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Write in NFC01A1 memory by i2c protocol in Python

Hi, I work on the NFC01A1 and want to write in the M24SR with i2c protocol in python. My goal is to put a URI in, "abc.com" in this example. Here, I will put only the 3 important parts of the code, Erase Message Length, Write Message, Write Message L...

0693W000001sv5KQAQ.jpg
TDufo.1 by Associate
  • 1003 Views
  • 3 replies
  • 0 kudos

Resolved! Are "NFC TAG type2 - NTAG213" compatible with X-NUCLEO-NFC03A1? Is this dev shield able tomanage NTAG213 password?

Hi, I am using X-NUCLEO-NFC03A1 and NXP NTAG213 Mifare Ultralight. I chose this kind of TAG because they can be protected by password. I downloaded all files like user manual, etc... about NFC03A1 but I couldn't find any informtion about password wri...

SDel.19 by Associate II
  • 2843 Views
  • 4 replies
  • 0 kudos

Resolved! External Amplifier for ST25R3911b

I designed an amplifier to increase power up to 5 w at the output to achieve larger reading distance,however once it operates at its full power i get no readings and when i reduce the output power to 200-400 mW i get readings however the performance ...

Ak.2 by Associate
  • 1244 Views
  • 4 replies
  • 0 kudos

Resolved! Approach for low power design

Hello,My design must be very low power consuming. So, I am intended to reach 50 uA while waiting for a card by using the Tag detection mode.Is there any other approach so as to decrease those 50 uA while waiting for a transponder?Reagards, Ramon

Jhern.1 by Associate II
  • 663 Views
  • 1 replies
  • 0 kudos

Resolved! Dev kit and roadmap for CR95HF

Hello,I have used the dev kit PLUG-CR95HF-B for the CR95HF, but it seems not to be available anymore.I want to use it for a new development and I need to confirm some points before.What is the roadmap for CR95HF?What is the ercommended devkit for CR9...

Jhern.1 by Associate II
  • 613 Views
  • 1 replies
  • 0 kudos