ST25 NFC/RFID tags and readers

Ask questions and find answers on ST25 NFC/RFID tags and readers, including connectivity implementations and antenna design.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST25R3911B reception fast mode not working

Hello. I'm currently working on a RFID research project using 2 ST RFID chip : ST25R3911B and ST25DV64K. The reader is the discovery kit with a home-made antenna to suit to the project constraint. The external filter has been redesigned and transferr...

mdesc by Associate II
  • 1155 Views
  • 5 replies
  • 0 kudos

Resolved! ST25R3911B errors when combination of two tags

What I'm doing is to perform anticollision with 1 or 2 NFCA tags present.When performing anticollision with just one tag, the function does never report an error and allways find 1 tag correctly.When performing anticollisiion with two tags:There are ...

0693W000007E3p3QAC.png
EBadi.2 by Associate II
  • 1405 Views
  • 6 replies
  • 0 kudos

Resolved! ST25R3911B ERROR FRAMING in reception

Hi,i'm trying to perform a communication with an ISO14443-A smart card using the X-NUCLEO-NFC06A1 expansion board. The smart card supports the following bit rate: 106, 212, 424 and 848 kbit/s according to the ATS received. If i negotiate with the ...

PDe G.19 by Associate II
  • 3096 Views
  • 15 replies
  • 0 kudos

Resolved! Hi. Can anyone tell me how to get started building the ST25R3911-DISCO example source? A Keil toolchain? Well that's helpful. Eclipse is preferred IDE? Thx

I've been working successfully with the STM8 MCUs, using ST-LINK, building, debugging. But I so far can't figure out how to get started building for the STM32L4x6, which hosts the ST25R3911-DISCO board.  Can't even pin down an IDE yet.

Resolved! Problems with ST25DV16K and Android 8.0

Hi ST Community,I am having trouble to make a NDEF record in a ST25DV16k tag be recognized by Android 8.0, I already read both AN4910 and AN4911 and understood the limitations in Android 8.1 regarding the NDEF and CC headers, but my problem is that e...

0693W000007DO8rQAG.png 0693W000007DO9VQAW.png

Resolved! In ST25RU3993-HPEV , what are the accessories provided when we buy ? Datasheet of Antenna which is provided along with the EVM board.?

Hi all, When ST25RU3993-HPEV, what are the accessories provided along with the EVM could not find the information in the portal. Let us know any where it is specified. Specification and datasheet of antenna used in EVM (Provided along with EVM)

Prabhu1 by Associate II
  • 537 Views
  • 1 replies
  • 0 kudos