cancel
Showing results for 
Search instead for 
Did you mean: 

Schematic x-nucleo-ihm08m1 does not seem to the latest

Hos
Associate II

Hello,

I have the x-nucleo-ihm08m1 board and looking into the schematic I do not see the potentiometer R42 in there.

I bought my board recently from mouser.

The schematic i downloaded from the web page of the board (attached).

Thanks in advance.

1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

thanks for the info. Yes this part is missing but you can consider R42 connected to the "Speed" line.

BR

Giuseppe Scuderi

View solution in original post

2 REPLIES 2

Hi,

thanks for the info. Yes this part is missing but you can consider R42 connected to the "Speed" line.

BR

Giuseppe Scuderi

Cristiana SCARAMEL
ST Employee

Hello @Hos​ welcome to the ST Community.

Was Giuseppe' answer complete?

If yes please "Select as Best" for a faster search of solutions in the Community.

If you feel a post has answered your question, please click "Accept as Solution"