User Activity

Hello i want to implement a variable mechanical resistance using a BLDC.​So for example the shaft of the motor is turned by an external force and the bldc tries to counteract the force to the tune of e.g. 100Watt.​Since the bldc acts like a generator...
Hello,I have the x-nucleo-ihm08m1 board and looking into the schematic I do not see the potentiometer R42 in there.I bought my board recently from mouser.The schematic i downloaded from the web page of the board (attached).Thanks in advance.
Posted on August 13, 2017 at 20:46Hello people,My design has buttons on the pins that are normally used for the system x-tal (PD0 and PD1) and a button on PC13.my MCU: stm32f103c8This is the code generated by cubeMx:<code>/** Configure pins as * An...