2022-03-03 12:24 AM
hi I have the ihm08m1 how can I change from 1 shunt to 3 shunt if by default it is soldered on 1 shunt?
Solved! Go to Solution.
2022-03-03 01:39 AM
Simply set the solder jumpers J5 and J6 accordingly (next to R43/R45), i.e. both to 3sh:
Does it answer your question?
Regards
/Peter
2022-03-03 01:39 AM
Simply set the solder jumpers J5 and J6 accordingly (next to R43/R45), i.e. both to 3sh:
Does it answer your question?
Regards
/Peter
2022-03-03 01:46 AM
Hello @SDall,
the selection for single/three shunt configuration is made with J5 and J6 jumper.
You have to move the tin drop on the 3Sh side.
Fore more details you can refer to the user manual UM1996
2022-03-03 03:36 AM
do you have to do it with the welding machine?
2022-03-03 05:57 AM
Yes, J5 and J6 are solder bridges.