cancel
Showing results for 
Search instead for 
Did you mean: 

Ihm08m1 change shunt

SDall
Associate II

hi I have the ihm08m1 how can I change from 1 shunt to 3 shunt if by default it is soldered on 1 shunt?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Simply set the solder jumpers J5 and J6 accordingly (next to R43/R45), i.e. both to 3sh:

0693W00000KbFAAQA3.pngDoes it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Peter BENSCH
ST Employee

Simply set the solder jumpers J5 and J6 accordingly (next to R43/R45), i.e. both to 3sh:

0693W00000KbFAAQA3.pngDoes it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Cristiana SCARAMEL
ST Employee

Hello @SDall​,

the selection for single/three shunt configuration is made with J5 and J6 jumper.

You have to move the tin drop on the 3Sh side.

Fore more details you can refer to the user manual UM1996

If you feel a post has answered your question, please click "Accept as Solution"
SDall
Associate II

do you have to do it with the welding machine?

Yes, J5 and J6 are solder bridges.

If you feel a post has answered your question, please click "Accept as Solution"