Resolved! SPICE model for PT1000
Hello! I need a SPICE simulation model for thermistor(PT1000-A). Kindly help!
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hello! I need a SPICE simulation model for thermistor(PT1000-A). Kindly help!
Hello,My new NanoVNA-H4 arrived today. I immediately set out to update its firmware to the latest version (v1.2.29) but have been unable to get the DFuSe_Demo_V3.0.6 bootloader to "Choose" the DFU file (NanoVNA.H4.v1.2.29). I get a "This file doesn...
Does anyone here have a datasheet for part# SD1731-11? I see on website only datasheet SD1731 and SD1731-14. Does anyone know what the "dash #" stands for?
I am currently working on downloading an image into the LT-22222-L using the STM32 Flash Loader. While the download completes successfully and runs as expected, I am encountering significant issues with the application. It frequently crashes, and on ...
I am looking for the component number marked EVU T03 GP442 casing SMB.Thank you
Dear Support, Please advise the difference between part numbers STL23NM60ND1311 and STL23NM60ND. Verify their interchangeability as well. Can be replacements for each other. Thanks
Hello, I'm using STM8S208 to receive 16 bit data in SPI slave. The SPI_DR is 8 bits. The master FPGA is sending 16 bits data, otherwise don't have enough luts.Is there anyway to solve this?
How long do EEPROM memories used in HDDs retain all data at a temperature of 36°C?EEPROM, like flash, does the number of erases/writes have to do with the data retention time?2.5" and 3.5" HDDs use EEPROM or flash to store BIOS/firmware. What type of...
ST M29W640FT 70N6H flash Nor chip with 20 erase write stored in temperature 33-36C and no powered In this case, what is the most approximate and realistic estimate of years for it to retain all the information written on this chip? an approximate num...