Resolved! About the use of the M24C64-FMC6TG with the I3C bus
"Does the M24C64-FMC6TG have a spike filter that allows it to be mounted on an I3C bus and operate at maximum speed?"
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
"Does the M24C64-FMC6TG have a spike filter that allows it to be mounted on an I3C bus and operate at maximum speed?"
when I use vl6810 with 51 chip , the i2c use pull up to 1.8V 。all the init register is correctly, I Using an oscilloscope for detection ,It seems all correct。but it always wait at VL6180X_REG_RESULT_INTERRUPT_STATUS_GPIO here :while(!(VL6180X_Read...
Please help me to find equivalent to this IC AP239
Hi, When I start MotorControl Workbench_6.3.0 and select the example project "Electronic speed control on the B-G431B-ESC1 kit" and do nothing else except generate the code, I get these error messages with attachment.Am I missing a software package o...
Hi I'm trying to reuse some code that uses use std::fstream for file access.I have the FATFS working and can read and write files. like this:fr = f_open(&fil, path, FA_WRITE | FA_CREATE_ALWAYS);if (fr == FR_OK) {// Write text to the filefr = f_write(...
Hello everyone, I have problem with IC identification. Marking is D300I , 90A819. Pls let me know what kind of IC it is.Vcc pin i the 1st pin, and GND is 8th pin, that's all I know.
Hi,I am working with an STM8 Nucleo 32 board based on the STM8s207K8 microcontroller. I am trying to receive data from a NodeMCU dev board via UART. The NodeMCU board successfully receives data from the server, and transmits it, however when I try to...
hi,I am looking for an example .hex file for the M24M02-DR 2Mbit EEPROM (256k x8 format memory). Could you please point me to it?
Hello! I need a SPICE simulation model for thermistor(PT1000-A). Kindly help!