Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STVD problem! It gets really slow when compiling

Posted on May 10, 2012 at 14:25Hi,Im using STVD v 4.2.1 patch 2 on my STM8 project, the problem is when I want to compile, it gets stucked annoyingly for around 10 seconds then it starts to save first and compile the codings normally. I couldnt mana...

konay61 by Associate II
  • 1551 Views
  • 2 replies
  • 0 kudos

STM8S-discovery

Posted on May 10, 2012 at 16:07bonjour ,je travaille à STM8S-discovery en utilisant STVD je reçois toujours cette erreur lorsque vous essayez de démarrer une version de débogage:Starting debug session...-> Emulator reset (usb://usb)...done.Openi...

Firmware Helpfile

Posted on May 08, 2012 at 10:45Hello ST-Community, I'm searching for a special STM8S-firmware-helpfile. In this file all firmware-functions are listed with arguments etc.. I already downloaded this file a while ago. But I can't find it now. I hope s...

ldues by Associate
  • 1570 Views
  • 2 replies
  • 0 kudos

DMA with both SPI and UART

Posted on May 05, 2012 at 17:05Hi,I am facing problem in accessing DMA with SPI and UART.Only one communication is possible with DMA.When I am using UART DMA then SPI DMA is not working and vice versa.Can you please give any solution to this problem...

create file interruput

Posted on April 09, 2012 at 20:16i want to create a new source file for interrupt but I don't know how to do? Could tou help me????? STM8S105C6

mr239955 by Associate
  • 1182 Views
  • 2 replies
  • 0 kudos

STM8S Cannot write to TIM2->CCMR

Posted on April 26, 2012 at 18:51Hi, I have just recently started developing with the STM8S003F3P TSSOP20 device. I have been working through a number of peripherals, which have gone fine, but have now run into a roadblock. I am using the STVD with ...

fraser by Associate
  • 1522 Views
  • 2 replies
  • 0 kudos

ST6 programmer

Posted on April 26, 2012 at 14:44There is any hardware tools to can program the ST6 on a modern PC (i.e. without parallel port)? The USB to parallel adapter can be used? Thanks, Antonio #epromer