cancel
Showing results for 
Search instead for 
Did you mean: 

2 Ethernet interface

cfortier
Associate II
Posted on October 13, 2006 at 11:29

2 Ethernet interface

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
cfortier
Associate II
Posted on May 17, 2011 at 09:33

Hello guys,

I wish to use two independent Ethernet interface with the STR912x.

I was wondering if anyone made it and if yes some implementation guide will help.

May i connect 2 PHY to the MII of the STR ?

Thanks and have a great day.

jean-philippe23
Associate II
Posted on May 04, 2012 at 08:13

Hi Cofor,

I asked myself the same question, especially when both MII PHYs are on the same chip (like in the KSZ8863 from Micrel). Did you managed to find an answer?

Thank you very much.