Posted on May 17, 2011 at 09:33Hello guys, I wish to use two independent Ethernet interface with the STR912x. I was wondering if anyone made it and if yes some implementation guide will help. May i connect 2 PHY to the MII of the STR ? Thanks and ha...
Posted on May 17, 2011 at 09:32Hi guys, I've manage to establish a SPI connection with an external SPI-Slave in Motorola SPI frame format on SSP0. Here are my GPIO setting. GPIO_DeInit(GPIO2); GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO...
Posted on May 17, 2011 at 09:32Hi guys ! We've just finish our first prototype with at STR912. Unfortunatly the startup sequence don't work. Using JLink.exe, we have all the good JTAG signals (as show in JLinkARM.pdf) but the uC don't respond throug...