Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L152C6T6 EEPROM erasing problem.

Posted on April 24, 2012 at 10:20Dear everyone,When the updating stm8l make use of the swim , Everytime the EEPROM data was erased. I don't know this cause.The download tool is RFasher7. Of course was disable the Erase EEPROM option in this tool.

hansung by Associate
  • 1015 Views
  • 2 replies
  • 0 kudos

Programming STM8S via USB

Posted on April 16, 2012 at 09:13Hi,Is it possible to program stm8s mcu s via comport/usb with interface card(maybe max232 chip etc.)?I dont need debugging.Programming will be ok.What should I do for that?Can I use STVP with my custom interface boar...

STM8S Discovery and CCO

Posted on April 14, 2012 at 11:40 I am new at this so please be gentle with me :) I am struggling to get the CCO pin to output the current clock frequency and I'm struggling. I have checked out the examples in the STM8S library (version 2.1), in...

Nevyn by Associate II
  • 975 Views
  • 1 replies
  • 0 kudos

Custom Frontend tool for ST10Flasher.dll

Posted on April 12, 2012 at 01:32Hi everyone, I am new to the st10 tools. I am trying to create a simple tool to dump a hex file from an st10F269, and then later return it to the st10. I am using the st10flasher v2.02. I have the development kit tha...

roundsb by Associate
  • 802 Views
  • 0 replies
  • 0 kudos

UART2 RX TX initialization-how to use?

Posted on December 14, 2011 at 22:47Hello, I have problem with initialization UART2 in my project(STM8S105). Below you can see part of my code, what am i doing wrong? I'm trying to send sign to LCD display. ...void UART2_Cmd(FunctionalState ENABLE);...

pietruha8 by Associate II
  • 1396 Views
  • 1 replies
  • 0 kudos

Using GPIO pins for additional I2C ports

Posted on March 26, 2012 at 22:26Has anyone come up with a way to use GPIO ports as I2C? My current app uses an external I2C mux to make three I2C channels. I would like to replace this HW with independent I2C output from the STM8. So I would have t...

jeff69xr7 by Associate II
  • 1079 Views
  • 1 replies
  • 0 kudos

eStudio,VIPER25

Posted on April 07, 2011 at 07:29Dear friends, I need use the VIPER25, is there anybody working on that. Because eStudio no provision for VIPER25. If any application note also ok for me. #estudio #viper25

vkjayak by Associate
  • 1237 Views
  • 1 replies
  • 0 kudos