Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STR912: problem writing boot code to Bank0

Posted on December 07, 2011 at 22:48Okay, I've learned how to move code to Bank1, and it executes properly. After having some problems getting bank1 booting to work, we decided to instead try copying our firmware into an external Flash chip and val...

ST-LINK : COMM TIMEOUT

Posted on May 23, 2012 at 13:00I am using STVD 4.3.1 with ST-LINK and windows 7 32bit.Most times I try to enter debug mode I get COMM TIMEOUT ERROR.  Clicking STOP and trying again just results in the same error over and over again.The only way to c...

Stm32User by Associate III
  • 2314 Views
  • 3 replies
  • 0 kudos

STM8S003F3 program flash not unlocking

Posted on June 21, 2012 at 13:54 Hi all, I'm trying to write an update routine for an STM8S003F3, so that it can be updated over SPI. I'm pulling 128byte chunks of data from a routine in ram, then attempting to write them to the mai...

skirkham by Associate
  • 800 Views
  • 0 replies
  • 0 kudos

STM8L101xx SR1 Changing Problem

Posted on June 18, 2012 at 17:23Hi everyone,I have serious problem about TIMx_SR1 register. This register is  0x07 at the normal time. I finished my code and i am using timer3 everything is ok. Sometimes my timer3 working wrong and i found problem.T...

RIDE 7 - no STLink support ?

Posted on June 13, 2012 at 14:47I'm relatively new to Raisonance/RIDE 7 for STM8 , and wondering that it seems not to support the ST-Link debug adapter, only it's own RLink. Is this correct ? Sorry to say so, but I consider this either poor performa...

STM8 SPI Wakeup

Posted on June 03, 2012 at 07:04I am using the STM8S as an SPI slave device.  The protocol I am using has a fixed sized buffer and I was thinking about using this interrupt to reset the buffer pointers.  The data sheet suggests that this interrupt c...

Nevyn by Associate II
  • 1146 Views
  • 1 replies
  • 0 kudos

Defining table in Flash instead of RAM, IAR

Posted on June 11, 2012 at 16:36Hello, Wondering if anyone has been able to use IAR to put a table in ROM memory instead of the default RAM with init table.  I would like something like: code int a[] = {1,2,3,4,5,6} or int a[] @ ''abc'' = {1,2,3,4,5...

chealy by Associate
  • 1939 Views
  • 4 replies
  • 0 kudos

float rounding Cosmic compiler

Posted on May 10, 2012 at 13:01Dear all,I have some strange roundings with float values: for example when I write 0.05 in eeprom (calibration parameters) it becomes 0.049999997 when I read It.0.2 becomes  0,199999988.I use Cosmic compiler, I tried t...

jfelix by Associate II
  • 1717 Views
  • 4 replies
  • 0 kudos

How to use <stdarg.h> ?

Posted on November 10, 2011 at 08:56Hi all,I'm using USART and communicating via rs 232 protocol and trying to send formatted strings by using stdarg.h C library to use;va_list, va_start, va_arg, va_end..but I don't know which library is supposed to...

konay61 by Associate II
  • 3621 Views
  • 6 replies
  • 0 kudos