Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer1 reset on trigger

Posted on July 07, 2012 at 20:24I found something very funny/weird when using TIM1 to measure the frequency of a signal: Set TIM2 and TIM1 to use the same prescaler (e.g. 8). TIM2 is configured to generate PWM with period 10000, in this case resulti...

klaasdc by Associate III
  • 2350 Views
  • 4 replies
  • 0 kudos

fMaster > 16 MHz on STM8S207: running slower?

Posted on June 28, 2012 at 02:29Hi all,I'm moving a design from STM8S105 to STM8S207.I'm thinking of raising the clock speed from originally 16MHz to 24 MHz in order to get more MIPS from the core.However, for clocks > 16 MHz, the flash memory requi...

nholzem by Associate II
  • 1015 Views
  • 2 replies
  • 0 kudos

Problem with STM8S103 ADC

Posted on June 27, 2012 at 05:08I am using STM8S103 to measure three channels of voltage signals named vs12, vs5 and vs3 respectively. Timer 4 is enabled to generate interrupt every 10ms and three voltage signals are measured alternately. That is, i...

tangsg by Associate
  • 1190 Views
  • 2 replies
  • 0 kudos

Timer interrupt flag clear problem

Posted on June 21, 2012 at 10:27Hi.. We are using STR912FAW44 and keil 3 as IDE. We are using TIM0 in OCM1 mode with OC1 interrupt enabled.We are using a counter inside the interrupt, Interrupt count time is 100 ms, we have to measure 900 seconds, s...

gupta2 by Associate II
  • 1674 Views
  • 3 replies
  • 0 kudos