User Activity

Posted on September 26, 2016 at 15:20Hi.I have a project working with a STM32F2/F4. I want to upgrade this project a bit, adding a CPLD/FPGA to do certain tasks that actually is doing the micro.We have done a small test and it worked with a SPI and ...
Posted on July 18, 2016 at 11:48 Hi. I have added USB Host support for MSC. It is working ok with USBs under 4gb... but it is not detected properly with USB-sticks over 4gb. I'm using library version 2.2.0, microcontroller are F2/F...
Posted on July 11, 2016 at 10:34 I want to copy a function from Flash to RAM and RUN it. I know that IAR includes the __ramfunc type for functions that allows you to define a function in RAM but i dont want to use it for 2 reasons: ...
Posted on May 02, 2015 at 12:43 Hi I have started a new project. I need to set 3xSPI at max speed. I'm using the discovery board with a STM32F407VGT6. This board has a 8mhz christal. I'm using cube, it is a nice tool that i'm start...
Kudos from