Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems using STM8S Discovery Board

Posted on August 09, 2012 at 01:13Hi all,I am a total Newbie in STM8s. I recently purchased a STM8SVL Discovery Board and it worked fine. After that I had to develop an Application for my project so I broke the Controller Board, prepare a Hardware a...

Unexpected RTC Calibration changes

Posted on July 23, 2012 at 10:38Hi All,I'm using STM8L and trying to compensate the RTC in terms of the temperature changes. But the calibration value doesnt effect as the written on the Application Notes and Reference Manual. For example, when I si...

konay61 by Associate II
  • 5328 Views
  • 12 replies
  • 0 kudos

stm8S003 constants at a fixed memory address

Posted on July 27, 2012 at 14:00HelloI'm trying place constants at fixed memory address according to this link http://www.cosmic-software.com/faq/faq3.phpMy code is:#pragma section const {sver}const uint8_t SV_HIGH=1; const uint8_t SV_MID=2; const u...

janusz2 by Associate
  • 2092 Views
  • 4 replies
  • 0 kudos

stm8s105c6 i2c problem

Posted on July 25, 2012 at 16:49I used pe1 and pe2 pin for i2c but this pins not work normally now. i make high pe1 and pe2 but this pins always low but pe0 and pe3 can be high. how do i connect this pins for i2c? 

assert & Str2Int

Posted on August 01, 2012 at 16:21I am trying to use assert () to check amd make sure that my input is an integer.  I assign char choice[15]; u32 a; u8 n;  then I write n=Str2Int (*choice, *a); and it don't work, error bad argument type.   If I chan...

carnett1 by Associate II
  • 842 Views
  • 0 replies
  • 0 kudos

Problems with EWSTM8 of IAR

Posted on June 25, 2012 at 21:33I have a project with STM8L151 and I have a dozen of quality issues with EWSTM8. Since a few days ago, after the upgrade to Win7, I have been facing consantly crashes. It seems to me as it happens because of  LiveVie...

elil by Associate III
  • 1283 Views
  • 2 replies
  • 0 kudos

issue with stm8s207rbt6 and eeprom

Posted on July 24, 2012 at 15:13Hi, I'm using stm8s library 1.1.1.Cosmic C 4.2.10 Compiler.the mcu is stm8s207rbt6 I'm experiencing an issue writing a byte in the data eeprom while I'm receiving data on the uart3 (tried also on the uart1 and it's th...