Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST1CC40DR too hot on 3A

Posted on August 08, 2016 at 21:51Hi! I have made a scheme for CREE X-ML2 LED (with maximum output at 3A) in eDesign studio. But missed that IC loses 0.8w power at 3A and getting very hot quickly, then stepdown output current to ~2A. Is there any wa...

pavel2 by Associate
  • 1085 Views
  • 1 replies
  • 0 kudos

Power Consumption with Input NOT at Rail

Posted on February 02, 2016 at 23:22I am using the STM8S103K3.  The data specifies power consumption only with all inputs at the rail voltage.  Also the data sheet says to ''turn off schmitt input'' on adc input to save power.  These things imply th...

Measure Time duration between high and low pulse

Posted on August 13, 2016 at 12:55I am working on STM8S003K3 microcontroller. I need to calculate time duration between two pulses. One high pulse (1) and another low pulse (0). The pulses will be created using switch. Approximate time duration woul...

anuj by Associate II
  • 804 Views
  • 0 replies
  • 0 kudos

A comparison of C compilers for the STM8

Posted on June 15, 2016 at 10:18A comparison of the 4 most important C implementations for the STM8 can be found at:http://colecovision.eu/stm8/compilers.shtml It uses the current (mid 2016) versions of all 4 compilers. Only aspects of the C impleme...

ADC Sleep Mode

Posted on August 09, 2016 at 01:34Hi,I am wondering if there is a sleep mode for the ADC for the STM8S003f3 processor.I want the processor to sleep until ADC_CSR_EOC = 1 or sleep while ADC_CSR_EOC = 0I did see a WEI but I believe it is only for the ...

ghan by Associate
  • 962 Views
  • 0 replies
  • 0 kudos