Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using Eclipse and STVD with Cosmic

Posted on September 29, 2016 at 15:03Due to the CDT debugging issue this is a fair workaround for productivity (convenience due to Eclipse, issue tracking, git handling, doxygen (eclox) etc.)Google always helps, so I gathered all info I found and te...

hjs by Associate II
  • 1560 Views
  • 0 replies
  • 0 kudos

Getting Cosmic C setup with STVD

Posted on September 28, 2016 at 15:36I've downloaded STVD, installed it, Downloaded Cosmic C, installed it and downloaded en.stsw-stm8069.zip (standard peripheral library) Now. I cannot for the life of me get this thing working. I opened the .stw pr...

wfd by Associate II
  • 1220 Views
  • 1 replies
  • 0 kudos

no ST-Link detected *sometimes

Posted on September 23, 2016 at 19:24I'm using the ST-Link V2 as a programmer repeatedly.  Sometimes it returns no ST-Link detected when I try to program.  Unplugging the device then plugging it in again solves the problem. When its in this state, I...

Viper 26LD loosing regulation

Posted on July 02, 2016 at 12:44Hi, I have used eDesign to implement viper on my application. My specs are input voltage 70Vdc to 160Vdc / output 15Vdc (5.1W). For some reason, the viper 26LD is loosing regulation (when connecting to a load) - the o...

vitor1 by Associate II
  • 5928 Views
  • 11 replies
  • 0 kudos

Code example STM8L152C6

Posted on August 30, 2016 at 10:07Hi, I'm trying to find some code examples I can run though using the STM8L152C6 micro. I'm new to this so I wanted some proven code I can step though and make sure I understand all of the commands, can anyone point ...

USB dongle SPIRIT1 RF SP1ML-868

Posted on September 04, 2016 at 09:43Hello, I am interested in buying the 868MHz transceiver USB dongle. I realise it's evaluation only, but I was wondering if you could give me an indication of whether I could get it to work as an ordinary 868 MHz ...