Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Help with identifying a component

Hello,I'm a software expert, and ignorant in any hardware fields.I have some faulty air condition controller board, and need help with identifying some faulty component installed on it.Could you please tell me what is this EEPROM component (see pictu...

MMovs by Associate II
  • 10032 Views
  • 10 replies
  • 0 kudos

I can not read / write NFC tag (NfcV)

I am developing a mobile application for Android for reading and writing data on NFC. While working with the M24SR04 chip from ST, then everything worked. After the transition to the chip M24LR64ER (also from ST) - ceased.This can be done using other...

PPost by Associate II
  • 1370 Views
  • 0 replies
  • 0 kudos

IAR STM8S PROGRAM DEPLOYING

I am using IAR EMBEDDED WORKBENCH FOR STM8s. I am running a simple led blink program. But I am facing while deploying to device. It shows the message "FAILED​ TO LOAD DEBUGEE". Please answer about this issue.

SBadd by Associate II
  • 752 Views
  • 0 replies
  • 0 kudos

Resolved! STNRGPF01 related questions

Hello, I found a problem in eDesignSuite when i try to use STNRGPF01 (PFC boost interleaved IC).At input current sensing the ICS Target Voltage is 3.00V and in the datasheet the ICS Target Vltage looks like it is 1.25V (also in the Help section of eD...

0690X000006CBzZQAW.png 0690X000006CBzUQAW.png

STVD Software is not responding

Hi, I am using ST Visual Develop environment for programming of STM8S207, i am using 4.3.6 version. Problem is, whenever i give save command, STVD is halt and shown "Not Responding" My laptop configuration is Pentium Dual Core, 2.0GB RAM, Window ...