Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C EEPROM 24LC16b, 24LC65 problem ...

Hello,I have a problem with I2C eeprom 24LC16b and also with 24LC65. Altough the internal buffer is 16 bytes I can sent at once only 15 bytes (14 characters + 1 null char) and the same is aslo for 24LC65 (Instead of 64 I can store only 63 chars at on...

0690X000006D7ZPQA0.jpg
AGoog by Associate II
  • 4313 Views
  • 6 replies
  • 0 kudos

Good morning , I would like to know if it is possible to extract the schematic/ BRD of this component in order to speed my design? Thanks a lot for your help, Kindly, Mailys

As you can see in the picture, I don't the ability to extract with PSpice, furthermore when I save it as .PRJ, after downloading Orcad, if I try to open the .PRJ there is nothing but a text file inside. Text as below of the Prj file : <eDesignStudio ...

mCAZA by Associate
  • 1722 Views
  • 1 replies
  • 0 kudos

Resolved! Issue reading program data from the flash

Good afternoon, I would like to share an issue I’m facing with a stm8s105c4.A feature of our main application is to calculate a CRC of the entire program in the flash. Unfortunately, when I read flash data from addresses close to the instruction in e...

0690X000006D6h8QAC.png 0690X000006D6hDQAS.png 0690X000006D6hIQAS.png 0690X000006D6hNQAS.png

Cursor alway run to EXTI line when hold press button

Hi all,I have a issue about interrupt timer and interrupt button. When i alway press button. Run debug, cursor alway run to interrupt exti line. I change timer 2,4 or pin exti still error occur. When I comment TIM1_Config() i alway press button-->in...

TMai by Associate
  • 1554 Views
  • 2 replies
  • 1 kudos

Free IDE for STM8 development

HI ST Team,We are planning to use STM8S103F2 MCU for dimmer application like the STEVAL-ILD004V2 reference board. Do you have IDE we can use (for free) or we need to get Keil/IAR license?Regards,Walter

WMaca by Associate II
  • 2956 Views
  • 6 replies
  • 0 kudos