Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! EMI Filter for USB interface of STM32

We are using USBUF01W6 as EMI filter for STM32F207VCT6 in USB D+ and D- lines in Full speed mode and we have connected VBUS (5V) at pin 3.3V pin of USBUF01W6. Does this make sense to you?NOTE: This question and answer originated from a customer suppo...

Accordo5 (STA1295) tool chain

Hi, I have searched and could not find any information about the Accordo5 nor Accordo2 SOC in the entire community. Even the Accordo5 product page do not contain much information. I am at loss to where to get information about the complete tool chain...

PTEOH by Associate
  • 816 Views
  • 0 replies
  • 0 kudos

With the STM8s105c6 and the STM8af5288tay, both which I use. what is the correct way to initialize multiple i2c devices on the same SDA/SCL port. i.e. I wish to have a RTC, i2c LCD as well as an EEPROM on the same i2c port.

How for example do I initialize all 3 devices, where addressing and necessary parameters are concerned.  Any sample code or advice in this regard would be very welcome. (RTC : either PCF8563 or DS1307; I2C LCD with PCF8574 expander and 24c32 or 24c64...

MGoss.19 by Associate
  • 776 Views
  • 0 replies
  • 0 kudos

Error creating process for executable cxstm8

I'm using the Cosmic Software 4.4.9.0 in ST Visual Develop 4.3.12  I can't compile it.I try to install again but it showing same error.i tried to set root path correct like this C:\Program Files\COSMIC\FSE_compilers\CXSTM8.Can any one help me to solv...

tvenk by Associate II
  • 2097 Views
  • 1 replies
  • 0 kudos