cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, Can ECMF02-2AMX6 used for USB 3.0 application.

SN.10
Associate II

Can you also confirm how many pins have inbuilt ESD diode? According to datasheet its 2. But according to diagram in datasheet 4 pins have ESD.

Also suggest which choke is better for USB 2.0 and USB 3.0 application among these two.

ECMF02-2HSMX6 or ECMF02-2AMX6.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FGUIT
ST Employee

Hi,

ECMF02-2AMX6 is dedicated to USB 2.0, and it was not tested for USB 3.0.

For USB 3.0, we recommend:

  • for 1 pair, ECMF02-2HSMX6
  • for 2 pairs, ECMF04-4HSWM10, or ECMF4-2450A60N10

For USB 2.0 and USB 3.0, I recommend ECMF02-2HSMX6.