cancel
Showing results for 
Search instead for 
Did you mean: 

Can you suggest an alternate part for ECMF02-3HSM6. In datasheet of this part ECMF02-2HSMX6, it is mentioned for USB3.0 applications. can it be used for USB 2.0 as well

SN.10
Associate II
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
FGUIT
ST Employee

ECMF02-2HSMX6 can also be used for USB 2.0. On datasheet, fig 13 and 14 give USB 2.0 eye diagram with and without part, to show that it is OK for USB 2.0, and to show that impact on eye diagram is very low.

Hi,
Can ECMF02-2AMX6 used for USB 3.0 application.
Can you also confirm how many pins have inbuilt ESD diode? According to datasheet its 4. But according to diagram in datasheet 4 pins have ESD
Regards,
Shifali N
Hi,
Can ECMF02-2AMX6 be used for USB 3.0 application as well.
Regards,
Shifali N
FGUIT
ST Employee

Hi,

ECMF02-2AMX6 is dedicated to USB 2.0, and it was not tested for USB 3.0.

For USB 3.0, we recommend:

  • for 1 pair, ECMF02-2HSMX6
  • for 2 pairs, ECMF04-4HSWM10, or ECMF4-2450A60N10

For USB 2.0 and USB 3.0, I recommend ECMF02-2HSMX6.

Regards.

Fabrice G