Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hi, my name is Alejandro,I am working with an EEPROM M24C64-RDW6TP which when removing the power does not start correctly in certain cases.Every 100 or 150 reboots, this failure occurs.I would like to know if you can guide me to solve the problem, si...
Hello,I have a LDF File with one Master and 2 almost identical slave nodes. The slave nodes only differ in name and ID. For example:slave_1 subscribs to slave_1_state and slave_1_position.slave_2 subscribs to slave_2_state and slave_2_position. Now I...
We have incorporated the VNQ7003 automotive high side switch in out Control unit and have no success in making it work. We implemented all the design and operation steps described in the datasheet and technical references and still have no response f...
Our implementation of the SWIM protocol expects the "HSI clock is trimmed" bit in the SWIM CSR to be set after initialization. As UM0470 states, "At the end of the option byte loading, the HSIT bit in the SWIM_CSR is set by hardware."In a test with S...
Hello,We have STM8S105K6T6C parts with same COO = Malaysia and same date code but some have MSL listed as 2 on the manufacturing label and the others have 3 as MSL. The question is which MSL is the correct one or they are both correct? I couldn't fin...
Hi,I am using window 10 version. Initially STVD was working well. Now from few days its not working. Automatically workspace get deleted, not generated. STVD starts not responding error. Automatically get closed. I am using COSMIC compiler.Then later...
the DOS window says synchronization OK then gives a unknown exception then says ERROR and dosnt load code any ideas?
Hello community, I am trying to debug my STM32f103C8T6 bluepill board (probably using fake chip) on STM32CubeIDE but there is something goes wrong about both GDB and Local Server. In debug configuration, When I set debug probe to "ST-Link GDB Server"...