Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hi, I want to run STM8S003F with an external crystal.How do I use APIs in stm8_clk?Or in which material is it described?Regards, Gotoda
How to drive bicolor LEDs by one pin. I think turn off LEDs when setting GPIO input. But it is not. On pin high level. What is problem.
The datasheet does not explicitly call out maximum current that can be monitored with the "current_sense" pins but it appears to be 1.5A. Does that imply that this is also maximum continuous per output current that the part is rated to? Or is it 3.8A...
ST10F276Z5T3: Shelf-life, recommende storage conditions
Compiling main.c...cxstm8 +warn +mods0 +debug -pxp +strict -pp -ps -psa -pu -l -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\Hstm8" -clDebug\ -coDebug\ main.c#error cpstm8 stm8s.h:2525(12) missing ;#error cpstm8 stm8s_gpio.h:68(18) incomplete declar...