cancel
Showing results for 
Search instead for 
Did you mean: 

Booting Linux or U-Boot via USB boot on SPEAr320

hj
Associate III
Posted on April 26, 2013 at 09:15

Hello

Is it  possible to boot Linux Kernel via the  USB boot mechanism in the SPAEr320 CPU?

If yes, what tools are available to generate an image for a bootable USB stick? I hope to get at least a link to an approbriate application note.

Thanks

 Heinz

#usb-boot
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jonazaza
Associate
Posted on April 05, 2014 at 21:59

hi I am really having problems with uboot. I am using hyperterminal and a usb to serial converter. I press space bar just after a hard reset but nothing happens

Osto
Senior
Posted on September 22, 2014 at 15:10

I dont know, if you already solved you problem but you should test it with a pc with dedicated RS232 interface or with a RS-232 PCI-Card. Almost all USB->Serial interfaces are not working for this purpose. You will have a lot of problems.