Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cannot issue NMEA commands to the Teseo on STEVAL-STRKT01 over good CN503 UART link.

Hello ST,I’m attempting to integrate the STEVAL-STRKT01 into my system.I need to issue NMEA commands to the Teseo .I’m connected into the UART over CN503 (TX,RX,GND only) and I can see the serial chatter.For example, I want to Stop the STAGPS engine ...

M24512-A125 EEPROM ECC ON, OFF

Hello,I am an auto parts developer.I am using the M24512-A125 product.I am writing 1 page of address 128 bytes.I am writing the same data by 3 bytes.I am writing 42 bytes of different data.I am writing 42 bytes * 3 bytes = 128 bytes.I am using Nbytes...

0693W00000GWtIaQAL.png 0693W00000GWtMFQA1.png
Skim.3 by Associate
  • 1158 Views
  • 1 replies
  • 0 kudos

stnrgpf01 programming

Dear sir/madam,where is the right place to program stnrgpf01 online by edesignsuite? I logged into eDesignSuite but didnt see the choice of stnrgpf01.Thanks,Michael

明杨.1 by Associate
  • 1396 Views
  • 2 replies
  • 0 kudos

Using external editor (like vscode) with stvd?

I've been using vscode as my editor since the one in stvd seems to have features from 15 years ago. I have files also open in stvd since clicking on errors opens files. This means that when I switch to stvd from vscode I get the warning about files...

mchahn by Senior
  • 1022 Views
  • 0 replies
  • 0 kudos

What can possibly cause USBLC6-2P6 failure?

In our application USBLC6-2P6 is connected between a USB port and a processor STM32L4R5xx. The circuit is self-powered (Li-ion battery), and uses either PC USB or USB dc power supply for charging and communication. We find a number of damaged USBLC...

AVain.1 by Associate
  • 1691 Views
  • 1 replies
  • 0 kudos

Resolved! Datasheet MDE GP743

Hi, I have some part with broken ST diode with label MDE GP743. Is this product still exist? where can i look for technical data for this part? Thanks

KGuna.1 by Associate II
  • 2642 Views
  • 4 replies
  • 0 kudos