Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ECMF02-2AMX6 Bad Eye Diagram for USB2.0

Hi,we are using the ECMF02-2AMX6 in our USB 2.0 lanes. The traces on our board are quite short. However, the measured eye diagram of USB 2.0 was not good. The eye is very close to the limit especially at the rising part. Now I saw that in the datashe...

0693W00000JNBnpQAH.png
CBmn by Associate
  • 1657 Views
  • 2 replies
  • 0 kudos

Resolved! phantom breakpoint

Dear support,When debugging code in Attolic TRUEStudio I am facing a fantom breakpoint phenomena. Sometimes I see this report from ConsoleTemporary breakpoint   1, main () at ..\src\main.c:71   71 int ret = 0;   No breakpoint number 2.It's a sh...

LPola.1 by Associate II
  • 3351 Views
  • 7 replies
  • 0 kudos

Resolved! Would you confirm the STM8S207RBT3CRT can directly placed to the STM8S207RBT6C with no Hardware/firmware changes?

We’re using STM8S207RBT6C for our current production. Due to the on-going IC shortage matter, we're trying to source a alternatives that can directly working on our existing design without any hardware nor firmware changes. We were able to find s...

skim.1 by Associate
  • 961 Views
  • 1 replies
  • 0 kudos

How to configure Timer for STM8s as input capture compare and how to get the capture compare values in interrupt handler.?

I have configured the timer as below is its is correct and also in interrupt handler I am not getting time the values.static void TIM3_Config(void){ /* TIM3 configuration:  - TIM3CLK is set to 16 MHz, the TIM2 Prescaler is equal to 16 so the TIM2 co...

Tk.2 by Associate
  • 2470 Views
  • 1 replies
  • 0 kudos