Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! conditional transition to sleep mode

In many aplications i am using simple template, where interrupt routines (for example UART receive) raise flags (volatile variables) and main() function polling these flags and processing these events (for example parsing incoming UART charaters). I ...

Resolved! M95512-6RMP EEPROM Doesn't work below 2.6V

Hello,We are using M95512-6RMP with STM32WL5CC, we powered EEROM with STM32WLE5CC Pin. According to M95512-6RMP datasheet its voltage range is 1.8V-5.5V.I have attached our schematic of EEPORM connection.Please help us in this case. We want to use EE...

DBhut.1 by Senior
  • 2157 Views
  • 8 replies
  • 0 kudos

How disable VrefInt ?

Hi there,On a battery-powered board using the STM8l050J3, in order to reduce at the minimum the power consumption, in Active Halt mode and using RTC wakeup, (at a few tens or at most hundreds of uA) as indicated, I want to disable Vrefint.To do so, d...