Adding encryption for CANBUS communications using STM8S208.
Has anyone successfully implemented/encrypted data transmission over the CANBUS using an STM8S208? Are there libraries anywhere to assist with this? Thank you.
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Has anyone successfully implemented/encrypted data transmission over the CANBUS using an STM8S208? Are there libraries anywhere to assist with this? Thank you.
For example how can the IO pins be set for alternate function mapping to non-default pin. As per datasheet same alternate pin function is mapped to multiple pins. For example USART1_TX is shown to be available on PC3 and also PA2. By programming all ...
As the STM8S001J3 MCU has no Reset pin, How do I connect the MCU with ST Link v2 using SWIM pin for debugging?STLink V2 : STM8s001j3VDD : VDDGND : GNDSWIM : SWIMRESET : ?I have left the STLink V2's reset p...
Hello, I am trying to access all the 5 gpio pins out of FIVE Gpio pins I am accessing 4 gpio pinss i.e (PD6/PA1 ,PA3,PC5,PC6).------->Port d and port c are accessing normally but port b is not able to access. ------->As per data sheet if we use swim ...
Hi, i'm looking for ST9309 - 137651 Transistor data sheet or equivalent. I beleive this transistor is obsoltet now so i'm searching for an equivalent transistor. This transistor is on my Bose accoustimass powered subwoofer. appreciate any help you ca...
Dear all,I am using STM8S103F2 in one of my design. I have two main missions in the code.1- Convert analog signal into digital and do some action according to voltage level.2- Catch an external interrupt in both falling and rising edges.I realized mi...
Hello everyone,I recently bought a single STM8S105K4 to fiddle with. I've soldered it to a board and I'm trying to flash it using the stm8flash utility and an STLINKv2. I've made the following connections to the MCU: STLINK -- MCU RST -- PIN 6...
Posted on November 15, 2017 at 01:03This part is in end of life, but I still need to build the boards.... is there a replacement?Thanks!Patricio#vnh2sp30tr-e
Posted on March 15, 2006 at 14:04PSDsoft Express, Rlink, PSD813F1 -- error programming EEPROM section
Worked in burst mode from 50V HV, then lower output voltage till 120VAC input, and almost totally powered off when input VAC above 135V. The ZCD resistive divider is 82 kOhm and 12 kOhm. Transfomer has 100 turns, 7 and 7 turns respectively. Lpri abou...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.