cancel
Showing results for 
Search instead for 
Did you mean: 

A bug in 91x_gpio.c

seawwh
Associate II
Posted on February 11, 2007 at 10:19

A bug in 91x_gpio.c

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
seawwh
Associate II
Posted on May 17, 2011 at 09:36

When use P9 as output port, should init the GPIO9 as follows

GPIO_DeInit(GPIO9);

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_Alternate=GPIO_OutputAlt1;

GPIO_Init (GPIO9, &GPIO_InitStructure);

if run this program step by step, we will find that:

SCU->GPIOOUT[GPIO_Number]=?? // GPIO_Number is 9 !!

But the range of SCU->GPIOOUT[] is 0..7,

SCU->GPIOOUT[8] and SCU->GPIOOUT[9] are not exist!!

I think should add the (1) statment in GPIO_Init function.

/**********************************************/

void GPIO_Init(GPIO_TypeDef* GPIOx, GPIO_InitTypeDef* GPIO_InitStruct)

{

/* Select pin direction */

u8 PinNumber = 0;

u8 Counter = 0;

u8 GPIO_Number = 0;

GPIO_Number = GPIO_GetGPIONumber(GPIOx);

if(GPIO_InitStruct->GPIO_Direction == GPIO_PinOutput)

{

GPIOx->DDR |= GPIO_InitStruct->GPIO_Pin;

}

else

{

GPIOx->DDR &= ~GPIO_InitStruct->GPIO_Pin;

}

for (Counter = 0; Counter < 8;Counter++)

{

/*Search pin number*/

PinNumber = (GPIO_InitStruct->GPIO_Pin & (1 <

if((PinNumber >> Counter) == 1)

{

if (GPIO_Number

{

/*Output ALternate 0*/

SCU->GPIOOUT[GPIO_Number] &= ~(0x3 <

if(GPIO_InitStruct->GPIO_Alternate == GPIO_OutputAlt1)

{

/*Output ALternate 1*/

SCU->GPIOOUT[GPIO_Number] |= 1 << (Counter *2); // (2)

}

if(GPIO_InitStruct->GPIO_Alternate == GPIO_OutputAlt2)

{

/*Output ALternate 2*/

SCU->GPIOOUT[GPIO_Number] |= 0x2 << (Counter *2);

}

if(GPIO_InitStruct->GPIO_Alternate == GPIO_OutputAlt3)

{

/*Output ALternate 3*/

SCU->GPIOOUT[GPIO_Number] |= 0x3 << (Counter *2);

}

}

/*Type configuration: PushPull or Open Collector*/

SCU->GPIOTYPE[GPIO_Number] &= ~(0x1 << Counter) ;

if(GPIO_InitStruct->GPIO_Type == GPIO_Type_OpenCollector)

{

/*Open Drain configuration*/

SCU->GPIOTYPE[GPIO_Number] |= 0x1 << Counter;

}

/*IP Connected disable*/

SCU->GPIOIN[GPIO_Number] &= ~(0x1 << Counter) ;

if(GPIO_InitStruct->GPIO_IPConnected == GPIO_IPConnected_Enable)

{

/*IP Connected enable*/

SCU->GPIOIN[GPIO_Number] |= 0x1 << Counter;

}

}

}

}

[ This message was edited by: seawwh on 07-02-2007 16:06 ]

[ This message was edited by: seawwh on 11-02-2007 09:33 ]

amira1
Associate II
Posted on May 17, 2011 at 09:36

Hi seawwh,

This error will be corrected in the next release v1.2 of the library which will be available next month.

Thank you and best regards,

mirou

aloisp
Associate II
Posted on May 17, 2011 at 09:36

Hi seawwh,

many thanks for having found this bug. I have been trying to use the I2C peripheral of my mcu for weeks, but without success. I use the STR912FW44 and on this mcu, the I2C interfaces are located on port 2. I was using ports 8 and 9 at the same time, and because of this bug, I2C would not work :(

Your post just gave me the missing hint... Thanks a lot.