Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C EEPROM 24LC16b, 24LC65 problem ...

Hello,I have a problem with I2C eeprom 24LC16b and also with 24LC65. Altough the internal buffer is 16 bytes I can sent at once only 15 bytes (14 characters + 1 null char) and the same is aslo for 24LC65 (Instead of 64 I can store only 63 chars at on...

0690X000006D7ZPQA0.jpg
AGoog by Associate II
  • 3220 Views
  • 6 replies
  • 0 kudos

Good morning , I would like to know if it is possible to extract the schematic/ BRD of this component in order to speed my design? Thanks a lot for your help, Kindly, Mailys

As you can see in the picture, I don't the ability to extract with PSpice, furthermore when I save it as .PRJ, after downloading Orcad, if I try to open the .PRJ there is nothing but a text file inside. Text as below of the Prj file : <eDesignStudio ...

mCAZA by Associate
  • 1237 Views
  • 1 replies
  • 0 kudos

SPWF04SA - UART_IRQHandler issue

Hello,I am developing a program with a WiFi socket user interface. I can communicate with the module using the Socket Test App. I give a certain command and my MCU does something. I generally found this to work fine until it came back after running ...

Resolved! Reading data from Socket Client

Hi, I am using the IDW04A1 with an STM F401RE MCU. On my program I want to be able to read data from a socket client, so I can essentially tell my MCU to run certain tasks over Wi-Fi. The problem is, all the Socket Read API just return the status of ...